Hello,
I designed a PFC converter which has the following features :
Vinac = 85V~130V (Typical input voltage is 115Vac)
Frequency = 400Hz ~ 800Hz. ( go from 400Hz to 800Hzn, avionic power supply)
Vout = 260V/ Poutmax = 150W.
I m using the controller UCC2818.
My issue is about the current harmonic distortion. I want to know if there is trick that exists to improve the distortion during the current crossing of zero.
I used your mathcad file and your note application to choose peripheral component (voltage and current loops).
bellow the current waveform @Pout=400W, Vin=85V, Vout=260V.
The waveform is correct except when the current is crossing zero.
I tried to change current loop component, it allows to improve the current waveform and harmonic distortion but it is not enough to meet the specifications.
Thank you for your help.