This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53318: Maximum OCP and its tolerance

Part Number: TPS53318


Hi~

As datasheet mentioned "For the TPS53318 device, the OCP threshold is internally clamped to 10.5 A. The recommended RTRIP value for
the TPS53318 device is less than 150 kΩ.".  May I know 10.5A is minimum or typical or maximum.

Current tests are up to 12A, will it hurt TPS53318?

According to electrical characteristics, the OCP tolerance is around 16.67% for full range temperature.

If 10.5A is typical value, 12A (scope maximum value) will be fine I think.

Could you please provide your opinion and clarify the question?

Thank you so much!

Tiger