Part Number: TPS7A52-Q1
Hello,
I have a question about input and output capacitor requierements. Datasheet says "The TPS7A52-Q1 is designed and characterized for operation with ceramic capacitors of 22 μF or greater (10 μF
or greater of capacitance) at the output and 10 μF or greater (5 μF or greater of capacitance) at the input. Use at
least a 22-μF capacitor at the input to minimize input impedance."
- For the input is 10uF OK like first sentence explains or we need 22uF?
- What is the sense of "10 μF or greater (5 μF or greater of capacitance)"
Thanks
Regards