This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

best buck controller to achieve close or even 100% duty cycle

Other Parts Discussed in Thread: LM5117, LM5166, LM5165, TPS54060

I'm looking to use a buck controller to achieve current regulation for a battery charger. My input supply is already voltage regulated and will be suitable to directly connect to the battery. However I must ensure I have current limiting. Having seen the interesting article on the LM5117 as a precision current regulator (snva609.pdf), this seemed like a possible solution.

However I am limited by the max duty cycle of the IC, having a minimum off time of 320nS to recharge the bootstrap. Even at lower switching frequencies I can not achieve better than 97% max duty cycle and I don't think it is possible to circumvent the min off-time even if I opted for an external charge pump.

I have also considered using the COT non-sync PFET buck switch to get 100% duty cycle, but this causes huge variation in output currents, due to the cycle by cycle current control.

I would like to have the predictable freq operation of a sync buck controller but use current sensing in the primary feedback loop. However I can not find any IC that seems to allow operation very close to or better still 100% duty cycle. I would also like to avoid using a buck-boost topology for simpilicity's sake.

Could TI make any recommendation.

Thanks

Aidan