This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2490: Puzzle me

Part Number: TPS2490
Other Parts Discussed in Thread: LM5069

Using  WEBENCH® TPS2490, the maximus number of "Output Current Limit" can be filled with 10 (Amps). It means the board's normal working current is 10 Amps or during the hot-swap period the current is 10A and after hot-swap period passed, the current can increase to 15 Amps or more?

My situation is that I want to use the function of hot-swap and my board's working currents can finally reach about 15 Amps.

According to it,can I use the chip tps2490?

Thank you!