This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28780: Can the UCC28780 be uesed as Active Clamp Forward?

Part Number: UCC28780
Other Parts Discussed in Thread: UCC2897A,

Hello,

Application: 70W PD converter paired with the TPS2373-4 for a 30V output.
Default used part is the  UCC2897A in active clamp forward configuration.

What is the limitation for the UCC28780 to be used in Forward converter versus Flyback?
If it can be used, should one expect better efficiency numbers (delats control driven)?

Thank you

Cosmin P.