Hello,
LM5020 OUT pin has 1A peak capability. My understanding is 1A peak rush current flows if capacitor is connected at OUT pin. Is my understanding correct?
In Electrical Characteristics, Iout = 50mA when high side on, Iout = 100mA when low side on and shows the drop voltages.
Does this mean OUT pin driver DC capability is 50mA and 100mA? Can we think ok LM5020 is enough capability to drive MOSFET input capacitor? There are smaller and larger input capacitor existing. I would like to know MOSFET loea will be no issue or not ussually.
Best regards,
Toshihiro Watanabe