This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24650: Help support on BQ24650 Issue

Part Number: BQ24650


Hi Team,

My customer is using BQ24650 in new project, but they met issue. Schematic as attached, input voltage is 11.7V and the MPPT is set to 17.75V. These is no battery at the output port, but sometimes these will be about 11.6V at the output port, sometimes not. If these is 11.6V, this voltage will hold for a long time. Seems randomly happen, do you have some suggestion or idea for this abnormal issue? Thanks a lot!


 

Best regards,

Sulyn