This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC2808A-2Q1: OUT Low Level and High Level

Part Number: UCC2808A-2Q1


Hi,

What is the OUT Low Level and High Level voltage at VDD=5V? 
The datasheet shows the spec at VDD=10V, but I couldn't find the spec at 5V.

Best Regards, Taki

  • Hello Taki,
    The data sheet parameters for the UCC2808A are characterized with a VDD = 10V.
    However if your are using the UCC2808A-2Q1 with VDD = 5V you can use the limits :
    VOL = 0.5V (nom) and 1V (max) with Io = 100mA and
    VOH = 4.5V (no) and 4V (max) with Io = 50mA

    Regards
    John