Hi, Can i make schematics of TPS22965 as ATTACHEDTI-QUERY.pptx
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Murugavel,
Thanks for reaching out on E2E!
Based on your schematic, if the ON pin, VBIAS, and VIN are all connected to the same input supply, the device might not have sufficient time to power up the internal circuitry (charge pump, gate voltage, etc). Therefore, the controlled slew rate can't be guaranteed. Is it possible to keep the ON pin on a separate enable line, or does it need to be connected to VIN? In order to guarantee the slew rate performance, ON must be toggled after VIN and VBIAS have reached steady state.
Thanks,
Arthur Huang
To find the latest information on Power Switches, visit www.ti.com/powerswitch
Hi Murugavel,
You can try including an RC delay on the ON pin if leakage isn't a concern. If inrush current isn't a concern for your downstream load, you can keep the circuit the way it is, and VOUT will follow the voltage on VIN.
Thanks,
Arthur Huang