This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76930: Schematic Review after failure analysis

Part Number: BQ76930

Hi team,

About 1% failure rate has been found in the production of customer.

After FA, it is found that Pin 3, 6, 7 and for some others Pin 3, 6, 30 is short.

So customer need some suggestions for their design.

Could you please provide a contact window, then I could provide the schematic and FA report to you by email.

Thanks.

Robin

  • Hi Robin,
    Pins 6 and 7 are TS1 and CAP1, these are associated with temperature measurement and boot.
    Pin 30 is ALERT, generally expected to go to an MCU.
    In general avoid sending overvoltage to a pin, avoid opportunity for coupling signals onto the lower voltage signals.
    Looking forward to receiving the schematic through internal email.