This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53355: Use VREG pin as enable source

Part Number: TPS53355

Hi Experts,

My application is 12V transfer to 3.3V, loading 20A.

Besides dividing from 12V, can I use "VREG" to enable TPS53355 itself? Is there any risk or limitation?