Hi Team,
need some help with the below questions:
I have some questions related to the 32KHz crystal and HFCLKIIN oscillator requirements for the TPS65920 and for the OMAP3515/30.
32KHz crystal
- According to the crystal requirements from the TPS65920 datasheet it needs crystal shunt capacitance of max 1pF. This requirement is hard to achieve (most of the crystals have typical 1pF shunt capacitance (1.5pF max). My question is if this requirement (1pF max) is essential or I can use crystal with typical 1pF shunt capacitance (1.5pF max)?
- Load capacitance: I don't understand the demand on the datasheet. At the crystals datasheet this parameter is 12.5pF max (or 9pF max) is it enough?
- At the TPS65920 datasheet table 11-4 (attached to this mail) there are some requirements that I don't understand and no crystal datasheet has such characteristics (pin to pin capacitance, input voltage, internal capacitor on each input, parallel input capacitance). Can you tell me how can I handle such requirements?
HFCLKIN : we want to use 19.2Mhz oscillator.
At the OMAP3515/30 datasheet there is a 3.6ns max requirement for the rise/fall time. At the TPS65920 datasheet the requirement is 5ns max.
In our design the OMAP will get the fast clock from the PMIC (that supply 2.6ns max rise/fall time at is output (according to table 11-12 at the TPS65920 datasheet).
My question is if I can use 5ns oscillator for the PMIC and rely that the PMIC will provide the OMAP with 2.6ns rise/fall time?