This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear colleague,
My power module customer asked
1. Whether UCC24612/UCC24610 could be used in Forward? Please describe it in detail.
I find a materials as below, why Control SR cannot control with UCC24612?
2. UCC24610 has SYNC PIN, which controls the secondary side by sampling the signal of the primary side. UCC24612 does not sample from the primary side. Is that a problem?
3. For UCC24612 reference design, I only found UCC24612 application in LLC and Flyback in TI.com. Do we have related reference design?
4. If customer want to use SR, do we have better reference design?
Appreciate it for your powerful support!
Best Regards,
Rock Su
Yes, up to 600kHz based on the datasheet, on a proper external circuit designed for SYNC, i.e., a proper signal to SYNC to make GATE turn off.
In applications, the power losses have to be evaluated carefully to make trade-offs between targeted efficiency and switching frequency.