Hi,
When the Charge current is over Chg Current Threshold and either over Chg Inhibit Temp High or under Chg Inhibit Temp Low , XCHG and CHG_INH never change they are (0).
When the Charge current is under Chg Current Threshold and either over Chg Inhibit Temp High or under Chg Inhibit Temp Low , CHG_INH does change to a (1).
Is there something that is needed to enable this feature to work?
According to document SLUA664 sections 2.2 and 2.3 this should work.
Chg Inhibit Temp Low = 0 C
Chg Inhibit Temp High = 40 C
Temp Hys = 5 C
Chg Current Threshold = 50mA
Thank you for your help