Hi,
I use BQ76925 for 3 cells.
Voltage measurement (VCOUT) are very stable and accurate.
However, current measurement (VIOUT) are not as expected. VREF is 3V, SENSEN is connected to VSS via RC filter (2x1kohm & 0.1uF as recommended in datasheet's table 27).
Rsense is 50mOhm.
At zero current, measured VIOUT is very noisy, the output is 20xx mV (Gain=4) and 22xx mV (Gain=8). When current>0, both VSENSEN and VSENSEP are changed. It's also strange that measured VSENSEP<VSENSEN for discharge current. I inspected code to ensure that I_AMP_CAL=0 to measure VSENSEN and I_AMP_CAL=1 to measure VSENSEP already.
I have no clue to start troubleshooting. Any suggestion?
Thanks,