Dear Sir,
I'm planning to use LM5041 IC for my new project, but while going through the schematic of the AN-1299 LM5041 Evaluation Board, I found diode D11 (CMPD2838-NSA) which is connected to Vcc.
I have following doubts regarding the use if D11 in the circuit:
1. The Input Output isolation will it have any effect.
2. What is the actual purpose of the diode in the circuit.
3. Upto what Max frequency can i use this topology ( as per datasheet it can go upto 1MHz), but atleast can i go upto 900KHz for the buck side, so 450KHz for Push Pull.
Thanks and Regards,
Nesh