This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27542-G1: Do the learning cycle before or after GPCRb update.

Part Number: BQ27542-G1
Other Parts Discussed in Thread: GPCRB

Hi,

      In SLUUB65A mentioned 5 steps as follow to complete prior to using a gauge with a battery.

1. Determine the ChemID.

2. Perform the learning cycle.

3. Test the gauge and optimize.(gpcra/gpcrb)

4. Finalize the golden file.

5. Program and test the PCB.

    In GPCRB manual mentioned to create gg file as follow 3 setps

1. Program chosen chem ID

2. Export .gg file or .gg.csv file

3. Rename the file regardless of format to gg.csv

 My question are

   1. Why the learning cycle is before GPCRB. My confuse is the GPCRB report will overwrite the Ra table, why the learning cycle are not peforme after GPCRB.

   2. About GPCRB manual, the gg file that to be upload is just need to program chem ID and the other parameter hold default value, or the other parameter need to set and learning. 

Thanks.