This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5041: LM5041 load sharing with UC2907

Part Number: LM5041
Other Parts Discussed in Thread: UC2907, UCC29002

Dear Sir,

Is it possible to implement load sharing in LM5041, also i have following doubts:

1. How to use UC2907 with LM5041 is it possible at 900KHz

2. Is there any solution from which I can limit the reverse current from the output side if I parallel with another power supply with same output voltage. with output current rating of 20Amin