This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61029: Maximum Output Current for TPS61029

Guru 29720 points
Part Number: TPS61029
Other Parts Discussed in Thread: TPS61020, , TPS61025, TPS61027, TPS61026

Hi Team,

I understand TPS61020 has 1.5A current limit and TPS61029 has 1.8A current limit of adjustable output.
The datasheet shows graph of "Maximum Output Current" for TPS61020 as the following however there isn't graph for TPS61029.



Do you have the same graph for TPS61029?
My customer wants to know "Maximum Output Current" for TPS61029 under Vin=1.2V, Vout=5V or Vout=3.3V in particular.

Best Regards,
Yaita