This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100: Error messages when creating Golden Image files

Part Number: BQ34Z100
Other Parts Discussed in Thread: BQSTUDIO, , EV2400

Hello,

I'm using bqStudio 1.3.80 with an EV2400.  The 9S9P LFP pack uses the bq34z100-G1 chip and I'm trying to create the Golden Image files.  When I click on "Create Image Files" I see the message "ROM command results returned invalid checksum" in the lower left corner.  I then see the message "java.lang.ArrayIndexOutOfBoundsException: 5" in the lower left corner.  I have restarted the bqStudio software several times but still get these messages.

Can someone help me create the Golden Image files without getting these error messages?

Thanks, Kevin