This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM7705: Guard band of the 4mV ripple relative to Vout

Part Number: LM7705
Other Parts Discussed in Thread: LM27761

All,

When looking at section 6.6 of the data sheet regarding min and max for Vout, I would like to know if these numbers are already guard banded accounting for the 4mV typical ripple?  If they account for the ripple; then can you confirm the Vout min and max numbers are the absolute limits when using the part under the same conditions as specified in the data sheet. 

Thanks,

HSG 

  • Hi HSG,

    The 4 mV value on page 1 is a typical only, with further details on page 4 and 5 of the D/S.

    You can also see figure 5 and 6 which show how the ripple varies.

    The LM27761 is a similar device, whose D/S shows lower ripple.
  • Hi Chris,

    Thanks for the quick response and I do understand the 4mV ripple is typical. However what I am trying to understand is when the data sheet shows the maximum or minimum Vout and states then that "All limits are specified by testing or statistical analysis" then I would not expect these Vout values to fall below or above the Vout min or max specifications as the limit should account for the ripple. Is my understanding correct?

    Thanks,
    HSG
  • Hi HSG,

    It's not entirely clear what you are referring to. Can you give an example?

    The output voltage spec, on page 4, is the DC level of the output voltage--what you would read with a meter. The output ripple, with no min/max, is an AC spec. These are independent.
  • Hi Chris,

    Your statement is clear. However a team member was reading a voltage on the output above the maximum voltage as stated in the data sheet. They asked if it was related to ripple causing the higher than expected voltage. I do not believe it is related. I believe it is that the current is higher or lower than the -20mA within there circuit and thus this is why they are seeing a voltage beyond the limit as the limit is specified for when there is a -20mA current.

    If you agree with my assessment then I can close this thread.

    Best,
    HSG
  • Hi HSG,

    If you need debugging help, then please ask for it first. I'd like a waveform of Vin, Vout, and the load current to assess things.

    Yes, the voltage will rise further if the load is higher.