I have used the part value of the Detailed Design Procedure at the page 21 of the datasheett.
Mode, ISET2 and CE are HIGH with a 6volt 5A source at input.
The data sheet exemple resistor value should get a 1A charge current. But actually whe I plug a batterie with 4.03V ISET1 and ISET2 LEDs are on which represent precharge state.
also accordly to the exemple, the precharge curent is 100mA but in my case the charge current is 500mA.
I really don't know what is going on.
Please help me :)