This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1663: Pin define

Part Number: TPS1663

Hi,

Here are some question about TPS1663:

1. In TPS16630-32EVM, pin 24 is Vin and pin 19 is Vout, but in datasheet, these 2 pins are all NC, which one we should follow?

2. in TPS16630-32EVM, all NC pin are connected to GND, can I just leave them floating?

3. Why connect them to GND? Is there any reason?

Thank you.

C.T.