hey,
I am using the BQ24195L to detect the nature of the device that is connected to my phone.
So I have connected the phone to my host pc using a usb cable (by only connecting the D+ and D- pins) , and i have used a splitter to plug the same usb cable into the BQ24195L which will generate the vbus and the Ground pins to the phone and will read the D+ and D- pins.
When the D+ D- bus is connected to the BQ24195L ( in order to detect whether it s connected to a charger or to a host) the communication between the host and the phone in this case , would not be properly established (USB device not recognized ).
Do you have any idea how to fix it so we could be able to connect the phone to the host and to use the BQ24195L as a host/adapter detector ?