Other Parts Discussed in Thread: TPS2065
I have tested my prototype board with a TPS2065D on it.
T = 25°C; Vin = 5V; Rload = 10 Ohm; -> 500mA.
Referring to the datasheet, Rdson should have a value of 100 mOhm.
That results in an expected drop of 50mV between IN and OUT on the TPS2065.
I have 10 test candidates with following dropvoltage between IN and OUT on the TPS2065D:
- 1x 75mV (150 mOhm)
- 1x 90mV (180 mOhm)
- 5x 150mV (300 mOhm)
- 1x 200mV (400 mOhm)
- 2x 300mV (600 mOhm)
None of the values is in the expected area. And many of them are very much larger than expected.
Is it possible that I have got a bad charge of TPS2065D?
Or what is the reason for these values?