This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5180: LM5180 - EVM with smaller transformer

Part Number: LM5180

Hello Team,

Among the transformers you have evaluated, the one that has been chosen on the LM5180EVM-S05 is relatively too big for the application I'm looking at.

Optimal would be an height lower than 10mm, in the range of 6mm.

Setup is the same as the EVM but the current will be up to 100mA.

Any recommendation is welcome

Thanks

SunSet