Other Parts Discussed in Thread: UCD90SEQ48EVM-560
I am able to configre the UCD9090 about power on sequencing on the eval BOARD aws per my own board (under design) . I am able to configure UCD9090 uhrough USB cable throgh PC. In my actual board does not support USB interface. Only support I2C interfae. I have Ti supported USB adapter 2006. It supports I2C interface.On my board I have placed 10 pin header foer SCL and SDA and Alert and PMBUS_control.
Unfortunately the evalboar UCD90SEQ48EVM -560 supports 14 pin header where as UDB adaptors 2006 supports 10 header ( and that is why I am not able to use USB adaptor. Do you have any eval board of UCD9090, that supports 10 pin header only
After configutration through eval board. I have to save the file in which format ?? so that that file will be used for download config file though I2C adaptor ? Is there any procedure for creation of config file ( for downloafg image through I2C bus.
Please let me know.