I'm seeing some vague and contradictory info regarding layout of the LMG1205. On one hand, there's AN-1112, which says the following on page 6:
"2. A copper layer thickness of less than 1 oz is recommended to achieve higher solder joint stand-off. A 1 oz. (30 micron) or greater copper thickness causes a lower effective solder joint stand-off, which may compromise solder joint reliability.
3. For the NSMD pad geometry, the trace width at the connection to the land pad should not exceed 2/3 of the pad diameter."
On the other hand, I'm considering the design files for TI's LMG1205 evaluation board, LMG1205HBEVM. That design shows the following:
1. Specifies 2oz copper on all layers, including the component layer.
2. Uses NSMD pads, but uses wide polygons to connect to the pads, some of which are at least as wide as the pads.
Obviously since the LMG1205 is made for high power density DC-DC converters, it's very convenient to use larger copper features than. But are we supposed to entirely ignore AN-1112? What guidelines are we meant to follow for the LMG1205?
Also, do the copper weights mentioned above refer to starting or finished thickness (including the plating)?
Regards,
Mike