Good morning
I'm trying to design a driver for a CREE COB led and I'm wondering if LM3404 is suitable for this purpose or if you can suggest to me some more specific component.
I read attentively the LM3404 data sheet aveilable in your site and I repeated the calculation sample with my data but some resuts make me unsure.
In particular I don't understand why the inductor ripple current, in case of short circuit (ΔiL(led short)) in my calculation path comes smaller than Il (peak) while in the data sheet at the steps [29] and [30] page 24 is the opposite.
In addiction, calculating the output capacitor, I don't understand the difference between ΔiL and ΔiF and if the target tolerance ripple current of 100 mA p-p indicated after step [31] is suitable for the COB led I intend to drive.
Down here i put my calculation path
| Input voltage: | 20 | Vin [Volt] | 1,34E-10 | cost | ||
| LED forward voltage: | 17,5 | V0 [Volt] | 0,4 | inductor ripple curront increase | ||
| LED current: | 0,75 | IL [Amp] | ||||
| Switching frequency: | 3,00E+05 | Fsw [Hz] | ||||
| RON =V0/(1.34 E-10*Fsw) | 440298,5075 | RON [ohm] | 470000 | Ron comm | ||
| fSW =V0/1.34E-10*RON | 281041,6005 | Fsw comm [Hz] | ||||
| tON = 1.34E-10*(RON/VIN) | 0,000003149 | ton [sec] | ||||
| ΔiL = 0.4 *If | 0,3 | ΔiL [Amp] | ||||
| LMIN = ((VIN - VO)*tON)/ΔiL | 0,000028341 |
|
3,30E-05 | uH L comm | ||
| ΔiL= ((VIN - VO)*tON)/Ltip | 0,257645455 | [Amp] | 3,00E-05 | uH L comm | ||
| ΔiL= ((VIN - VO)*tON)/LMax | 2,83E-01 | [Amp] | 3,50E-05 | uH L comm | ||
| ΔiL= ((VIN - VO)*tON)/LMin | 2,43E-01 | [Amp] | ||||
| IL(peak)=IL+0,5*ΔiLMax | 8,92E-01 | [Amp] | ||||
| ΔiL(led short)= ((VIN - 0,2)*tON)/LMin | 1,89E+00 | [Amp] | ||||
| IL(peak )=IL+0,5*ΔiLMax | 8,92E-01 | |||||
| Rsns=(0,2*L)/((If*L)+(V0*tsns)-(((Vin-V0)/2))*ton) | 0,270571089 | ohm | ||||
The mentioned COB LED is a CREE XLamp CXA1507-0000-000F0YE435F with
Vf 17,5 V
If 750 mA
Thank you very much for the help
best regards
Federico Polidori
mail kikopoli12@gmail.com