This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/BQ76940: BQ76940 Sample current

Part Number: BQ76940

Tool/software: Code Composer Studio

while the BQ76940 wakeup from sleep mode,an error current would occurred during the first single current sampling,but after this current sampling,the continuous current is ok.

  • Hi User,
    When waking from sleep and turning on the CC, the write must synchronize to the timeline of the device, then the device must have 250 ms to acquire the value. It may take approximately 500 ms from wake to have a valid value. Once a value is present it will be updated every 250 ms, reads between that interval will return the last value.