This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZM33606: UVLO formula for 14V lockout

Part Number: LMZM33606

Hello,

I was reading the datasheet for the LMZM33606 on page 21 Table 7 you have provided a UVLO for 10V and 15V.

But some of our batteries have minimum discharge at 15V and others at 13.5V.

I was hoping that we can implement a lockout at around 15.5-16V for one battery and for the other battery 14-15V.

But I was looking for a formula which I could use to work this out but there isn't one.

Or is the UVLO very accurate with tight tolerance to lock out at exactly 15V?

Would I be able to get help and advise on this.

Best regards

Mohammed