This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23861: Manual Turn-on to device w/o Signature

Part Number: TPS23861


I'm having trouble getting the TPS23861 to power devices that don't have a PD signature, even though the TPS23861 is in manual mode.  I have three different types of devices. Those types are connected using 4-pair UTP (CAT5), single-pair UTP and single coax cables.  The single-pair UTP  devices turn on and stay on.  The CAT5 devices start to turn on, then shut off, repeatedly (the code runs in a loop).  The coax devices don't seem to turn on at all.  I'm trying to find the settings to force a port to turn on and stay on when  no signature is detected.

  • Hi Thomas,

    What's expected the port current for the CAT5 device and coax device? For keep a TPS23861 port on, during the inrush stage (60ms after port is on), the port current should be lower than 425mA and during normal operation, the port current should meet valid MPS signal(a minimum dc current of 10 mA or a 10-mA pulsed current for at least 75 ms every 325 ms). Can you please take waveform capturing port voltage(Drain-Vpwr) and port current(current gun at the pairs having current going through) and check TPS23861 fault registers(0x00, 0x02 ~0x0B )? I can help with the analysis. Thanks.

    Best regards,
    Penny
  • Hi Penny,

    Thanks for your quick response.  I'll get some waveforms, but I can answer some of your questions now.  The normal operating current for both units is about 30 to 35 mA.  The Start/ILIM Event Register (0x09) does show a start fault for the ports in question.  I should mention that nearly identical units that have a signature chip start up without any problems.

    Thanks again,

    Thomas

  • Hi Penny,

    Here's a shot of the (very brief) turn on waveform.

    Thanks,

    Thomas

  • Hi Thomas,

    I can't tell what's happening with the limited information. Can you please take waveform capturing port voltage(Drain-Vpwr) and port current(current gun at the pairs having current going through) and all register dump(0x00 to 0x0B)? Thanks.

    Best regards,

    Penny

  •  Hi Penny,

    The image I sent earlier is Vpower relative to the drain voltage.  Now I'm attaching the voltage across the current sense resistors (0.255 ohms).  I'll send the register dump later.

    Thanks,

    Thomas

  • Hi Penny,

    Here's the register dump.

    Address Value
    0x00 0xC1
    0x01 0xE4
    0x02 0x01
    0x03 0x01
    0x04 0x00
    0x05 0x00
    0x06 0x00
    0x07 0x00
    0x08 0x01
    0x09 0x00

    The port in question is port 1.  Ports 2 & 3 are powering devices with signature chips and working normally.  Port 4 has a different problem.  I think the FET is shorted on.  That's not my concern now.  Port 1 has the waveforms I sent earlier.

    Thanks,

    Thomas

  • Hi Penny,

    The following register dump might be more useful.

    Address Auto Man1 Man2
    0x00 0x88 0xC3 0xC1
    0x01 0xE4 0xE4 0xE4
    0x02 0x00 0x45 0x01
    0x03 0x00 0x45 0x01
    0x04 0x0F 0x00 0x00
    0x05 0x0F 0x00 0x00
    0x06 0x00 0x00 0x00
    0x07 0x00 0x00 0x00
    0x08 0x00 0x01 0x01
    0x09 0x00 0x00 0x00

    The second column lists the register values after the port was in automatic mode. The third column shows the first readings after setting the port in manual mode. The last column shows the values after repeated readings in manual mode.

    Thanks,

    Thomas
  • Hi Penny,

    I just realized that I hadn't included all the registers you requested, so here's an updated register dump.

    Addr Auto Man1 Man2
    0x00 0x88 0xC3 0xC1
    0x01 0xE4 0xE4 0xE4
    0x02 0x00 0x67 0x01
    0x03 0x00 0x67 0x01
    0x04 0x0F 0x00 0x00
    0x05 0x0F 0x00 0x00
    0x06 0x00 0x00 0x00
    0x07 0x00 0x00 0x00
    0x08 0x00 0x01 0x01
    0x09 0x00 0x01 0x01
    0x0A 0x30 0x30 0x30
    0x0B 0x00 0x00 0x00

    The columns are the same as my earlier post.  Any ideas?

    Thanks,

    Thomas

  • Hi Thomas,

    The Man1 and Man2 columns show the port 1 has start fault which caused your port being failed to turn on. In manual mode, the PD doesn't need to pass detection and classification, but it has to follow the inrush current limit. The inrush current limit is described in datasheet section 8.4.2 inrush protection. Basically, the PD current during inrush stage(the first 60ms after turning on of TPS23861 ) has to be lower than 425mA. If not, the PSE will shutdown the port after inrush times out. Thanks.

    Best regards,
    Penny
  • Hi Penny,

    The current appears to be well below 425mA. The second waveform I sent shows a voltage of around 20mV across the 0.255ohm current limit resistors. Am I missing something?

    Thanks,

    Thomas
  • Hi Thomas,

    Can you please connect your load to TPS23861EVM-612 and hook up the GUI? I want to isolate the problem. Thanks.

    Best regards,
    Penny
  • Hi Penny,

    We are now convinced that the problem is that the current is limited to less than 100mA initially and power limited until the voltage rises enough  (over 27V).  The foldback during inrush curve (figure 57 in my version of the datasheet) shows the limiting.  Our devices try to turn on (and draw well over 100mA) at fairly low voltages (well below 20V).  Is there a way to change the turn on to allow higher current at lower voltage?

    Thanks,

    Thomas

  • Hi Thomas,

    You are right the figure 57 shows the current limit during inrush stage. Since TPS23861 is designed based on IEEE standard, the inrush current can not be adjusted.  You can read figure 57 from right to left. During turn on,the port should be in 44V to 57V range. If the current exceeds 425mA, the MOSFET will try to limit the port current. MOSFET limits the port depending on the actual current level. Usually our customers add some delay at the load side to make sure the PD doesn't draw 425mA during inrush based on IEEE standard. Thanks.

    Best regards,

    Penny

  • Hi Penny,

    Thanks for your response.  The devices at the load side are established products that we can't change.  We're hoping to use the TPS23861 to replace a chip that'll soon be discontinued.  We expected that in manual mode the TPS23861 would just turn on without trying to meet IEEE requirements.  We have found a possible workaround.  If we reduce the current sense resistors enough, the chip reads a lower current and turns on our load devices.  We haven't settled on the final value, but it'll probably be between 0.1275 and 0.170 ohms.  We can adjust our user interface to give the correct current readings.  We are not concerned about limiting the power sent to the load devices.  We have current limiting fuses on each output port, so we aren't concerned about overloading the TPS23861.  Are there any reasons we should not use the TPS23861 this way?

    Thanks,

    Thomas

  • Hi Thomas,

    If you don't care IEEE compliance and shifted current protection level, it is OK to reduce the current sense and turn on the port in manual mode(without detection and classification). Thanks.

    Best regards,
    Penny