This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92602-Q1: Maximum output drive power of each channel

Part Number: TPS92602-Q1


What is the maximum output drive power of each channel of TPS92602-Q1? I am not able to find the  information related to maximum drive  power in  the data sheet? where I can find this information. It would be grateful if anyone can support me. As  I am planning  to drive a LED with Vf=52V and If=1.3A per channel and input voltage Vin =24V.