This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RE: BQ51050B: Wireless Charge Not Terminating

Hi Bill Johns,

Thanks for your support. I want to clarify one doubt. As per datasheet calculation Rilim = R1 (330) + Rfod (1.5K) = 1.8K should set maximum charge current around 170mA. But when I have measured the battery charge current using Digital Multimeter in Ammeter mode the maximum charge current was coming around 130mA. Rterm = 5.6K will set termination current >40mA, but termination happens when ammeter current reaches zero. Also termination is not happening sometimes and charging continues with current between 0 to 1mA. I think this is causing the battery protector IC to shutdown mode due to battery overcharging.

Regards
Hafiz