This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22925: TI Load Switch Crosses

Part Number: TPS22925
Other Parts Discussed in Thread: TPS22990, TPS2552, TPS25221

Hello,

I am trying to find the closest TI cross for a few Load Switch parts. I have found what I think would be the closest matches but I am looking for verification or whatever else would be a good fit. I don't have any customer specifications for these parts, I am just looking for a closest match to these comp parts.

1. SLG5NT1477VTR - www.mouser.com/.../SLG5NT1477r122_01062014-876356.pdf

Possible TI cross- TPS22925

2.G5244A31U

www.gmt.com.tw/.../EDS-5244.pdf

Possible TI cross - TPS29929D 

Any input would be appreciated! 

Thank you, 

-Olivia Morell

  • Hi Olivia, 

    Thanks for reaching out on E2E! Please find the answers to your questions below:

    1. SLG5NT1477VTR: 3-5.25V, 6A, 9.8mΩ Load Switch"

    [AH]: To go against the SLG5NT1477V, I think the TPS22990 would be the best option. The TPS22990 can support up to 10A, with a lower Ron, and contains additional features such as Power Good (PG), Quick Output Discharge (QOD), Adjustable Slew Rate (CT), and a larger VIN range than the SLG5NT1477V.

    2. GMT G5244: 2.7 - 5.5V, 2.5A, 120mΩ USB Load Switch:

    [AH]: Since the G5244 has a current limit feature, I suggest looking at the TPS25221 or the TPS2552/3. These devices offer better Ron, fast RCB response time, and adjustable current limit. 

    Let me know if you have any additional questions!

    Thanks,

    Arthur Huang