HI
TPS7A6601GDGNRQ1 , can i use it for 7V output
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi PYTsai,
No the TPS7A66-Q1 family of devices is not rated for a 7 V output. The recommended operating conditions define the region where the regulator is designed, characterized, and tested for operation. 7 V exceeds the recommended operating conditions for Vout.
We do have several automotive qualified LDOs that can achieve a 7 V output. Here is a link to our parametric search that is already filtered for automotive linear regulators that are able to have at least a 7 V output. You can add additional filtering criteria based on your application as well to narrow the list further.
Very Respectfully,
Ryan