This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24210: USB / Solar charger lipo

Part Number: BQ24210


Hello,

I need to create a USB/Solar charger using the BQ24210. The solar panel is a 6V 0.6A panel. 

As i don't have a thermistor for the battery, i don't know what to do with VTSB and TS.

I've made the following design, for Icharge 800mA. But from what i've read i should have instead connected TS to VTSB only with a 1K resistor in between.

If you have a design that work and are willing to share, i'll appreciate greatly.

Thanks for any feedback.

Simon-Pierre