Hello,
My cosutomer is wondering what the accuracy of VREF is at the FB pin in PFM mode. I saw a similar question posted earlier last year on this topic for the foloowing condition:
- measurement conditions
・Input voltage 1.8 V to 3.2 V
・Output voltage 3.3 V
Link:
Does the 775mV to 825mV apply for all input and output conditions or just the ones Seishin asked about?
Thanks,
John