Hi,
I'm trying to use TLC5951 with AMPMAFB-33.0000 MEMS oscillator for Grayscale PWM clock signals, connected to GSCKR/G/B in parallel. As soon as the oscillator is connected to the TLC's pins, the clock signal breaks down, recovering after opening the connection again. So I wonder if the input pin's capacitances might be too high. Could you tell me the capacitances of GSCKR/G/B pins? In the datasheet it's only stated that the input current is maximum 1µA.
If this doesn't lead to a solution, do you recommend any spedcific oscillator IC to be used with the TLC?
Thank you very much for the support.
Best regards,
Tino