This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65150-Q1: DLY1/2 and FDLY pin setting

Part Number: TPS65150-Q1

Hi Team,

For TPS65150-Q1, several questions that need your help:

1. For DLY1 and DLY2, what's the max capacitor value limit that could be used ? Customer have one panel that need to set it as 60ms and 30ms, thus larger cap value need to be used.

2. For FDLY pin, if the fault detection time function is not used, the spec suggest connecting the FDLY pin to VIN. So between FDLY and VIN pin connection, should it be connected directly, or one small current limit resister like 1K ohm need to be used ? What's the min and max value for the resister value ?

Thanks.