This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC59116-Q1: Question regarding output management when severals are connected to one LED Cathod

Part Number: TLC59116-Q1
Other Parts Discussed in Thread: TLC59116,

Hi Team,

I currently use the TLC59116 for RGB management and I want to use it to manage one power LED (white or IR).

I see in the TLC59116-Q1 datasheet (page 31) that it is possible to use several outputs for one LED.

Regarding the power LED, I want to power it at 250mA by using 5 outputs with 50mA max for each.

For I²C management, do I have to set the 5 outputs at the same value (between 0 and 255) or can I set them with different value (i.e.: out0 = 255; out1 =60; out2 = 0 ...)? It is important for me because it is linked to LED current step.

If you need additional datas, don't hesitate,

Thanks in advance for your feedback

Baptiste,