Tool/software: Code Composer Studio
Hello Sir,
Previous Conversation i have ask you Battery Cycle Count related problem in which i ask that Battery Cycle count is Corrupted and according to your suggestion that in a second we should only read once. so i implemented the same and battery cycle count is not getting corrupted. but one further problem has occurred.As i put our machine on testing for battery after a charging and discharging battery cycle count should incremented by one but in this case our battery cycle count is incremented by two counts.for cycle first count is increased at 95% or above that and second count is incremented in between 20%-25%.So please could you tell us what precaution we should take so that we can not face the same problem.
Thanking you