Hello,
One of my customer came with the following questions,
There is a maximum output capacitance requirement for the linear regulators. (5 uF Max)
For 3.3V I have a separate DCDC converter. In the meanwhile the load of this separate converter changed to only one remaining IC, which has a small isolated power transfer inside. This IC recommends 10uF at input and at the output.
Charging the 10uF at the output may cause quite some peak load so that I think that I will need the 10uF on the input. (I did not get a recommendation back from the IC supplier if it is OK to reduce that to 1uF)
So when I move that load to the TPS65381, I would have to increase the capacitive loading to about 14uF. Can you give me a recommendation, if 15uF instead of 5uFmax is a problem on the TPS 3.3V LDO output?
There is some physical distance on the PCB, so there will be some milliohms of trace resistance at least.
Thanks in advance,
- Needhu