In my application the load is a DC motor which starts and runs for short bursts. This results in a high peak starting current (3ms rise time, 40ms fall) and then a short run time (Typically ~200ms to 1s). I see from the datasheet that the coulomb counter produces a complete reading every 250ms in ALWAYS ON mode, but it is not clear how effective it will be at integrating the pulse waveform I have described.
Is there a figure for the effective bandwidth of the current integrator? Or putting it another way, what is the minimum pulse width that will be captured?
Many Thanks