Dear Team,
My customer wants to use the UCC28780 without auxiliary winding for VDD, but rather have a dedicated VDD source:
- What components can be eliminate from the schematic (SWS, HVG, etc.)?
- How can I connect the VS pin?
Best regards,
Nir.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Team,
My customer wants to use the UCC28780 without auxiliary winding for VDD, but rather have a dedicated VDD source:
Best regards,
Nir.
Hello Ulrich,
Thank you very much for the information.
I have read the UCC28780 data sheet, and I like the many features it has.
1 & 2: Regarding the VDD and ZVS sampling, I understand that I have to use Qs, and that's OK.
3. Regarding the VS, I have an issue using it even when I have an auxiliary winding, since I need a CC/CV functionality down to 0V. I do not want the short circuit protection. Is there a way to configure the UCC28780 to have a 48V output that is current limited down to 0V? (I was planning on driving an opto feedback for CC/CV control).
I would like to have an active clamp flyback DC-DC isolated converter. I need a small, efficient, and quiet design.
Regards,
Yair