Part Number: BQ25895
I´m designing a handheld equipment with the BQ25895 to power an 15W led driver.
The wall adapter I intend to use is 5V 3.25A with a single li-ion battery capable of delivering over 10A discharge current.
From the datasheet it´s clear that PMID can suppy up to 3.1A at 5V (15.5W) but it´s not clear if SYS is capable of delivering 4 to 5 Amps at 3.7V (~15W).
1. Should I power the led driver from PMID or SYS?
2. For instance, when PMID is active and the minimum system voltage is set to 3.7V will VSYS be at 3.7V with VBAT at 3.2V (wall adapter not connected)?
3. When PMID is active the battery charging is suspended, right ?