Other Parts Discussed in Thread: , UCD3138
Tool/software: TI C/C++ Compiler
now,i want to write a code about LLC half-bridge circuit ,the device i used is ucd3138A, what should i do?how can i start?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Yes, you're right, it's not open loop. We've never actually done an open loop LLC code. It's problematic starting up in resonant mode, because the filter starts out with a zero in it's output and the DPWM never gets triggered, so it never triggers the filter.
I tried to do it once using preset and using force start on the Filter to put the values in, but I ran out of time before I got it working. So I'm not aware of any sample code for open loop for half bridge LLC.
With the closed loop code, since we start up in PWM mode, it's not a problem. The PWM mode gets things going so there's a good number in the DPWM when we switch to resonant mode.
What do you need it for?
I have designed llc circuits, I used code from ti,but no pwm output,so i wang tried openloop code to make sure the software no mistakes。
The LLC circuit i have designed,just like the UCD3138ALLCEVM150,I have used the LLC code from TI, but no pwm output, it didnot work. so i want a open-loop LLC code to debug my PCB.
If your board is the same as the EVM, it will support PWM mode at light load, so you can use an open loop PWM for testing. If you look at the UCD3138 video training, you can find a couple of different ways to make open loop DPWM signals. You will have to adjust the frequency and dead times for your application, but that's not very hard. In fact, using the first lab that exercises the DPWMs, you can even put out a static simulation of a point on the resonant curve, which is perfect for debugging.
i have used the code,it is pwm output is ok,but the topology is HSFB? i am not sure whether the training code can be used for llc
You will need to figure out what timing you need. In lab 2, you can put in whatever timing you need into the event registers.
I'd start out with a small on-time for both phases, assuming that your primary FETs are on DPWM0, make Event 1 maybe at 200 nsec, event 2 at event 1 plus whatever pulse width you want. Then make event 3 at half the period plus 200 nsec, and event 4 at Event 3 plus whatever pulse width you want.
In this static situation, you could put event 1 at zero, but in a dynamic system, you want to keep it out of the event update window at the start of the period.
You need to look at the timing on the scope and get it right before you apply power to the FETs.
OK, i will follow your steps to debug,try the code soon,thank you very much,