Other Parts Discussed in Thread: BQ24079T
Hi Expert
I use a 1000mAh battery to do test and set "direct charge control" function enabled, as log I can see the gauge control the 3 times discharge cycles then enable the charger to charge battery but I can not see the FCC has update.
Please advise how to set the bq34110 by direct charge control to get battery capacity learning.
Charge IC EVM : bq24079T
Gauge IC EVM : bq34110
the alert 1 pin drive a gate pin of 2N7002K the Drain pin to connect CE pin of bq24079T.
Attached enclosure file are log file and gg file for reference.
https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/196/bq34110-log-and-GG.7z