Other Parts Discussed in Thread: TLC5958
Dear TI experts,
After reading the application report for TLC59581, I have some questions that I would like to confirm about ES-PWM.
1. Is the multiplexing ratio which is 1/32 represents the 32-row scan of the LED matrix ? If it does, then if I want to drive 96x96 px display, will it require total of 18 pcs of TLC59581 to drive it with 1/32 multiplexing ratio just like illustration below ?
| 32x16 | 32x16 | 32x16 | 32x16 | 32x16 | 32x16 |
| 32x16 | |||||
| 32x16 |
2. In the 8+8 mode, and 7+9 mode, I observe that 7+9 mode will have higher visual rate, but the two of them will have about the same frame refresh rate ? Is there a method to improve the refresh rate because the one in tidu370 the refresh rate reach 60 Hz ? My calculations are provided below :
interval between segments (deadtime) = 0.1us
frefresh = 1/tsub-period
frame rate = 1/display-period
8+8 mode :
frefresh = 1/ [(257x32)/33MHz+31x0.1us] = 3963.3 kHz
frame rate = 1/[(tsub-period x 256)+0.1us x 254] = 15.475 Hz
7+9 mode :
frefresh = 1/[(129x32)/33MHz+31x0.1us] = 7800.87 kHz
frame rate = 1/[(tsub-period x 512)+0.1us x 511] = 15.22 Hz
3. How will cascading affect the refresh rate ? In tidu370, it uses 8 pcs of TLC5958 and cascade 4 of them but the refresh rate can still achieve 60 Hz
Thank you, looking forward to hearing your reply.
Regards,
Reno